Advanced Waveform Utility

Carriers > General Settings

Enabled

Power

Phase

Sample Rate

Number of Samples

Resampling Ratio

Frequency Offset

Repeat Number

Length

Smoothing Filter Frequency

Timing Offset

Enabled

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:[STATe] ON|OFF|1|0

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:[STATe]?

SCPI Example

 

Preset

OFF

State Saved

Yes

Range

ON|OFF

Initial S/W Revision

A.19.03

Power

Set the power boost level of the carrier.

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:POWer <real>

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:POWer?

SCPI Example

 

Couplings

Only applied on carrier mixing

This setting is applicable and displayed only when there are more than one carrier.

Preset

0

State Saved

Yes

Min

-130

Max

130

Initial S/W Revision

A.19.03

Phase

Set the initial phase of carrier.

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:PHASe <real>

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:PHASe?

SCPI Example

 

Couplings

Only applied on carrier mixing.

This setting is applicable and displayed only when there are more than one carrier.

Preset

0

State Saved

Yes

Min

0

Max

360

Initial S/W Revision

A.19.03

Sample Rate

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:SRATe?

SCPI Example

 

Notes

This value is the maximal value of all contained segments.

Preset

50 MHz

State Saved

Yes

Min

1e3

Max

128e9

Resolution

1

Initial S/W Revision

A.19.03

Number of Samples

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:SAMPle:COUNt?

SCPI Example

 

Notes

When a new waveform file is selected, the sample count will be got and assigned to this setting.

Preset

10000 Sa

State Saved

Yes

Min

1

Max

1024*1024*1024

Resolution

1

Initial S/W Revision

A.19.03

Resampling Ratio

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:RRATio <real>

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:RRATio?

SCPI Example

 

Couplings

When this value is changed, Sample Rate of Waveform will be changed too.

If Sample Rate Mode of waveform is manual, then Resampling Ratio of carrier can be changed manually.

Preset

1

State Saved

Yes

Min

0.1

Max

Depends on the sample rate and number of samples of imported waveform.

Resolution

1

Initial S/W Revision

A.19.03

Frequency Offset

Set the frequency offset of carrier.

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:FREQuency:OFFSet <real>

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:FREQuency:OFFSet?

SCPI Example

 

Couplings

Only applied on carrier mixing.

Preset

0

State Saved

Yes

Min

-64e9

Max

64e9

Initial S/W Revision

A.19.03

Repeat Number

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:REPeat:NUMBer <integer>

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:REPeat:NUMBer?

SCPI Example

 

Couplings

This setting can be changed only when carrier repeat mode is manual.

If carrier repeat mode is auto, repeat number is calculated based on current waveforms.

Preset

1

State Saved

Yes

Min

1

Max

1000

Initial S/W Revision

A.19.03

Length

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:TIME:LENGth?

SCPI Example

 

Couplings

With SCPI, only get action is meaningful.

Preset

0.001

State Saved

Yes

Min

0

Max

1

Initial S/W Revision

A.19.03

Smoothing Filter Frequency

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:FREQuency:COFF <integer>

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:FREQuency:COFF?

SCPI Example

 

Couplings

Only used for carrier mixing, when carrier is truncated, appropriated smoothing filter frequency is needed to smooth truncated signal.

This setting is applicable and displayed only when Carrier Repeat Mode is set to Manual and Repeat Number is greater than 1.

Preset

3000000

State Saved

Yes

Min

1

Max

128e9

Initial S/W Revision

A.19.03

Timing Offset

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:TIME:OFFSet <real>

[:SOURce]:RADio:AWU:WAVeform:CCARrier<carrier>:TIME:OFFSet?

SCPI Example

 

Notes

This setting is meaningful only when there is more than one carrier in waveform.

Preset

0 ms

State Saved

Yes

Min

0 ms

Max

10 ms

Resolution

1 ps

Initial S/W Revision

A.19.03

Welcome to AWU

AWU Overview

Waveform Settings

Segment Settings

Crest Factor Reduction Settings

Correction Settings